• RE: LT6600-10 : Chebyshev filter and Ripple Parameter

    Sorry, it is an error ! The good reference of the ADC is the following one: LTC2175-12.

    Regards,

    Philippe.

  • RE: How to properly and passively clock two ADCs from single encode clock source?

    What is the clock being generated by?

      The LTC2268 also comes in a quad (LTC2175) if you need four channels all synchronously sampling, that might be a better option. 

  • RE: Sample FPGA code for interfacing to LTC2192 device

    Verilogp2175_src.zip

    Here is the verilog code for the LTC2175/2268/2195 families.  It should be a a good starting point for you.  If you need an additional help, let me know.  

  • AD8039 noise issue

    In this project, we used Linear's high speed ADC LTC2175, LT6409(SE~Difference) as the driver. AD8039 as the first level amplifier and follower. Signal input Range: ±0.5V~±5V (i.e. Gain: 1~10); Input Freq: DC~60 MHz; When the input signal of AD8039 connected…

  • 2008-12-08 07:12:12     SPI and BF-561

    2008-12-08 07:12:12     SPI and BF-561

    Filip Vanalme (BELGIUM)

    Message: 66501   

    this item might already been discussed earlier. I looked into some forum discussions, but never found exactly what I'm looking for...

    I'm developing on a BF-561 board…

  • LTC2324-12

    I hope that I'm in the right place

    I have a question regarding the Linear LTC2324-12:

    I'm using the internal reference (my case is 2.048V) - can I use REFOUTx as an input for resistor division? please see the attached file configuration?

    Thank…

  • NVIC_SetPriorityGrouping(12);

    Hello,

    In ADI UART test examples we have:  

    /* NVIC initialization */

        NVIC_SetPriorityGrouping(12);

    but inside NVIC_SetPriorityGrouping() function is written:

    "

    The parameter PriorityGroup is assigned to the field SCB->AIRCR [10:8] PRIGROUP…

  • 2008-12-03 12:12:16     browsing svn source via web

    2008-12-03 12:12:16     browsing svn source via web

    Kyle Schlansker (UNITED STATES)

    Message: 66246   

    Is there a way I can view svn tree through the web?

    This page: http://docs.blackfin.uclinux.org/doku.php?id=version_control_systems&s[]=web&s[]=svn…

  • AD9172-FMC-EBZ: Files not found in Linux driver

    Hello, I am targeting the AD9172-FMC-EBZ and I seem to be missing some files from the Linux driver.

    Here is what is found I get:

    root@zcu102-ordwg:~# ls -al /sys/bus/iio/devices/iio\:device2/
    total 0
    drwxr-xr-x    5 root     root             0 Sep 19 00:45 .
    drwxr-xr-x    4 r…