• RE: LTC6409 DC-Coupling

    The LTC2158 has a common mode voltage of 0,8V (0.783V to typical), the amplifier needs to provide that or else you will need to provide blocking caps and pull up resistors to provide the ADC with a proper common mode voltage.  The input of the LTC6409…

  • 2008-12-08 07:12:12     SPI and BF-561

    2008-12-08 07:12:12     SPI and BF-561

    Filip Vanalme (BELGIUM)

    Message: 66501   

    this item might already been discussed earlier. I looked into some forum discussions, but never found exactly what I'm looking for...

    I'm developing on a BF-561 board…

  • LTC2172-12

    Hello,

    I'd like to ask some suggestion about how to connect the clock with this kind of ADC (LTC2172-12 65MSPS). Is not so clear for me how to choose the clock frequency (and so the kind of VCO) and how to connect it to ENC+ and ENC- (if some kind of…

  • NVIC_SetPriorityGrouping(12);

    Hello,

    In ADI UART test examples we have:  

    /* NVIC initialization */

        NVIC_SetPriorityGrouping(12);

    but inside NVIC_SetPriorityGrouping() function is written:

    "

    The parameter PriorityGroup is assigned to the field SCB->AIRCR [10:8] PRIGROUP…

  • LTC2324-12

    I hope that I'm in the right place

    I have a question regarding the Linear LTC2324-12:

    I'm using the internal reference (my case is 2.048V) - can I use REFOUTx as an input for resistor division? please see the attached file configuration?

    Thank…

  • LTC2313-12 SPI issue

    I am using an LTC2313-12 in combination with an ESP32 using (V)SPI functionality of the ESP32.  

    According to the description in the datasheet (https://www.analog.com/media/en/technical-documentation/data-sheets/231312fb.pdf -- p10/22 - Serial Interface…

  • 2008-12-03 12:12:16     browsing svn source via web

    2008-12-03 12:12:16     browsing svn source via web

    Kyle Schlansker (UNITED STATES)

    Message: 66246   

    Is there a way I can view svn tree through the web?

    This page: http://docs.blackfin.uclinux.org/doku.php?id=version_control_systems&s[]=web&s[]=svn…

  • Multiplexed 12 bit audio

    I have an application where the ADAU1701/2 would be ideal, but the lack of bit shift will be a problem, I have 2 input streams with each stream being audio packed as four 12 bit numbers (2x 12bit left and 2x 12bit right) I need to de-multiplex these and…

  • Electrical Characteristics of LTC2312-12

    Hi

    I don't understand what Absolute Input Range in LTC2312-12 data sheet as follows mean. Please let me know.

    Regards

    Hiroyuki