• LTC2157-14 conversion errors at 250MHz sampling rate

    I am using LTC2157-14 in a design.

    In the last production run (10 units) i get conversion errors on all boards when sampling at 250MHz.

    What i call a conversion error is a single sample with very high amplitude when measuring noise (shorted input), typically…

  • LTC2157 2-Tone IM3 at 140MHz?

    What is LTC2157 Two-Tone Input IM3 at 140MHz? 

    I don't see any IM3 info in the datasheet, and I only see one spectral plot with a 2-tone input around 70MHz.

    Are there more 2 tone plots or IM3 versus input frequency data available anywhere?

    Thanks.

  • 2011-01-10 14:14:47     workqueue

    2011-01-10 14:14:47     workqueue

    Chris Brissette (UNITED STATES)

    Message: 97302   

    I have been hunting a random lockup, happens about once a week. Seems like it has something to do with the using the ttybf1 uart.  I have been looking to where workqueue…

  • 2011-09-14 14:43:03     user spi

    2011-09-14 14:43:03     user spi

    Dario Bueno-Baques (MEXICO)

    Message: 103388   

    Hi everybody:

    I planning to develop an application for the bf537 stamp where is necessary to acquire some data from and ADC (16 bits simultaneous sample i.e like AD7655) make…

  • 2008-05-14 14:34:13     Memory Protection

    2008-05-14 14:34:13     Memory Protection

    Henning Manteuffel (GERMANY)

    Message: 55833   

    I connected an FPGA to the Blackfin address/data bus for accelerating arithmetic computations.

    Is there a way to unprotect certain addresses in user space so that…

  • 2008-01-14 14:07:12     ~~Many Thanks~~

    2008-01-14 14:07:12     ~~Many Thanks~~

    Kris Dickie (CANADA)

    Message: 49562    I think it's important to give the BF-uClinux support team credit. I run a support forum for my company as well (although much less traffic), and I know how demanding it can become…

  • 2011-03-14 14:18:22     Problem with CONFIG_DEBUG_EARLY_SERIAL

    2011-03-14 14:18:22     Problem with CONFIG_DEBUG_EARLY_SERIAL

    Timur Aydin (TURKEY)

    Message: 98924   

    I was debugging an intermittent boot issue with my blackfin BF537-0.3 board. I defined the CONFIG_DEBUG_EARLY_SERIAL option in the hope of getting more…

  • 2010-11-14 01:14:10     EZ-Kit for BF533

    2010-11-14 01:14:10     EZ-Kit for BF533

    Jawad Riaz (PAKISTAN)

    Message: 95825   

    Hi..

    I am trying to install linux on a EZ kIt for Blackfin....I have configured the host PC with linux GCC and other repositories...I need help on how to configure the toolchain…

  • 2008-09-26 14:14:15     uClinux 08r1.5 not compiling

    2008-09-26 14:14:15     uClinux 08r1.5 not compiling

    ashwin b (INDIA)

    Message: 62813   

    I am facing a problem in the last step: make

    Here is the error I am getting:

    cc -Werror -Wall -DHAVE_MKSTEMP -o cksum cksum.c crc.c print.c sum1.c sum2.c crc32.c