• 2008-12-08 07:12:12     SPI and BF-561

    2008-12-08 07:12:12     SPI and BF-561

    Filip Vanalme (BELGIUM)

    Message: 66501   

    this item might already been discussed earlier. I looked into some forum discussions, but never found exactly what I'm looking for...

    I'm developing on a BF-561 board…

  • LTC2324-12

    I hope that I'm in the right place

    I have a question regarding the Linear LTC2324-12:

    I'm using the internal reference (my case is 2.048V) - can I use REFOUTx as an input for resistor division? please see the attached file configuration?

    Thank…

  • NVIC_SetPriorityGrouping(12);

    Hello,

    In ADI UART test examples we have:  

    /* NVIC initialization */

        NVIC_SetPriorityGrouping(12);

    but inside NVIC_SetPriorityGrouping() function is written:

    "

    The parameter PriorityGroup is assigned to the field SCB->AIRCR [10:8] PRIGROUP…

  • 2008-12-03 12:12:16     browsing svn source via web

    2008-12-03 12:12:16     browsing svn source via web

    Kyle Schlansker (UNITED STATES)

    Message: 66246   

    Is there a way I can view svn tree through the web?

    This page: http://docs.blackfin.uclinux.org/doku.php?id=version_control_systems&s[]=web&s[]=svn…

  • Electrical Characteristics of LTC2312-12

    Hi

    I don't understand what Absolute Input Range in LTC2312-12 data sheet as follows mean. Please let me know.

    Regards

    Hiroyuki

  • PPI receive 12 bits

    Recently I made a board with a BF518 that used the PPI with a 12-bit interface.  I used the pins corresponding to D0-D11 and it worked fine except that I had to shift the data because it was zero-filled in the high bits.

    Is it possible to connect to D4…

  • AD9238 (12-bit) Converter

    Hi,

       We are evaluating the AD9238 12-bit converter.  This part is available in 12-bit (AD9238) and 14-bit (AD9248).

    We purchased the AD9238 evaluation board.  The board description is in the datasheet but that description and schematic is for the AD9248…

  • Multiplexed 12 bit audio

    I have an application where the ADAU1701/2 would be ideal, but the lack of bit shift will be a problem, I have 2 input streams with each stream being audio packed as four 12 bit numbers (2x 12bit left and 2x 12bit right) I need to de-multiplex these and…

  • AD7821 with 12 Bit Resolution

    We are using AD7821 ADC (8 bit) in one biomedical instrument. But, now to improve accuracy, we need 12 Bit ADC. Since we have current stock of PCB's where AD7821 is used, is there any ADC IC which is pin to pin compatible to AD7821 with 12 Bit resolution…