• Purpose of low pass filter on LTC2054 Amplifier

    Hello all,

    I am working on a design using the LTC2054 op-amp, I am planning on using this device to amplify a photodiode, on page 16 of the datasheet for the 2054, they list and example circuit for exactly this purpose, which consists of what looks basically…

  • LTC2050/1 and LTC2054/5 max. current on input pins

    Hi, 

    could you provide information about maximum current on input pins of subject opamps? Or the rule "5mA" can be considered here as good practice?  

    Something like it is provided for the part AD8603/7/9  in the data sheet, page 12, chapter INPUT…

  • RE: Voltage-controlled current source

    Do you have a preferred package type?

    LTC2050 or LTC2054 are related parts to LTC6081.

  • ADXL206 zero G shifting

    I'm using an ADXL206 in a board to detect the orientation of it, it should operate up to 150°C.

    I laid out two prototype boards and started a test up to 135°C, they worked fine for a couple of hours and then I noticed that on one board the X axis…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • RE: High voltage fully differential amplifier ( supply voltage >= +/- 30V )

    Hello Homan,

    Thanks a lot for the solution. I'll certainly try out the second circuit which looks easy with minimal components. 

    Could you please take a look at the attached datasheet of LTC6244, page 21? 

    It explains FDA from single ended opamps. I'm…