• LTC1983 burst mode

    what is the BURST MODE of LTC1983?

    How does it work?

    When does the BURST MODE used?

  • Bad output voltage of LTC1983-5

    Hello,

    I want to use the LTC1983-5 to generate -5V for to supply some microcircuits. Without load and without filter, I measure -4,869. After adding filter (LC circuit : 680µH / 33µF), the output voltage decrease dowon to -4.859 (but it's acceptable…

  • RE: Reliability Information Regarding Parts

    Hi Megan,

    LTC1983 reliability information is available on it's product page. FIT and MTBF in years is available in the reliability document. 

    Best Regards,

    Kristine

  • Application Circuit LT6550 RGB to Ypbpr - missing green

    I am working to convert RGBs from an arcade board into Ypbpr component video.  I am following the example schematic provided using two lt6550 to perform the matrix conversion.  After completing the circuit I do not have green, nor any colour using green…

  • RE: ADV3220 Supply

    The specifications for the ADV3220 are with +-5V rails.

    It is also spec'd at 0-12V rails but the real problem here is the video signals would have to be AC coupled and biased to ~mid-point for proper operation.  This is a more complex circuit.

    The…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • RE: Video DACs ADV7123-EP and ADV7393 output opamp driver circuit

    Attached is a app note on general video circuits including AC-coupling

      PDF

    For full galvanic isolation might be accomplished using video transformers however I do not have any experience with this path.  There are several transformer solutions used in…