• Compensator circuit of LTC1871 and LTC3704

    I plan to use LTC1871 and LTC3704, but unfortunately these regulators are not supported by LTpowerCAD. The reference manuals of these regulators are quite detailed to make quantity of FET, diode, impedances and boost capacitor, but I did not find any…

  • LTC1871 - Can I simulation AC analysis in LTSpice?

    I would like to design a power supply with LTC1871 and my question is can I simulation AC analysis in LTSpice with this IC?

    Best regards
    Adam Toth

  • RE: Thermal  runaway of LTC1871.

    What is your input voltage range, output voltage and maximum output current?

    Also, what was your load current and input voltage when you observed high current?

    BR,

    Goran

  • LTC1871重载时PWM占空比不连续

    应用LTC1871芯片搭建的16-21V输入;24V9A输出电路在9A重载时,PWM波形出现占空比不均匀的情况,比如前一个占空比40%,下一个周期仅有1%左右,周而复始,请问是什么原因造成的?

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • RE: .file_attr 1="1";

    Hi Gideon,

    Sorry for the delay in responding.

    The cause of the problem is "-file-attr CORE0" and "-DCORE0" both being included on the compiler command-line. Could you delete CORE0 from the "Additional attributes" in Tools Settings > CrossCore Blackfin…

  • RE: [????]??,????1

    This question has been closed by the EZ team and is assumed answered.
  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…

  • ADF7030-1

    Hello,

    I bought the ADF70301 - 433 EZKIT and I can't find, in the ADF70301 data sheet, the noise figure of the transceiver. 

    So I'm here to ask: how can i measure the noise figure of the ADF70301 using the 433EZKIT?

    Thank you for your support

  • ad7656-1

    I'm requesting the gerber files for this product mentioned above... is it possible to receive them. thanks,