• LTC1778 maximum inductor value

    What is the largest practical inductor value (10uH, 100uH) to be used with the LTC1778, specifically when used with light loads (10mA to 250mA)? I understand that the LTC1778 will drop back into discontinuous mode with light loads but has anyone studi…

  • LTC1778 voltage spikes destroy switching MOSFETs / Diodes; Similar measured at DC385A application

    Hallo,

    I have problems with existing LTC1778 circuits on our PCBs.

    Circuit is designed for 24V Input, Output 3.3V 5A.

    Basic functions are OK but we have complaints that synchonous MOSFETs (IRF7470 40V) or Diode (SD2114S040S5R0 40V) in parallel to bottom…

  • LTC1778 3V3 GENERATION

    Hello,

    I'm trying to make a local on-board voltage converter using  LTC1778. I need 3.3v Vout and 1A Iout. /Vin 5v

    I made some maths to get Ron and L, but Im not sure is this are correct or not, 

    I also need regulators for  1.8V and 1.1V same current…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032