Hi,
using ADV7611 with 8-bit YCbCr BT656 mode VID_STD=0x8, PRIM_MODE_GRAPHICS, 60Hz, OP_FORMAT_SEL=0 I can receive 640x480 progres 60Hz video.
I would like to increase color depth received by uC from present 16bits to 24bits.
It could be done by receiving…
Is there any IC, that can convert CVBS -> RGB24(8:8:8).
But in LQFP or, FQFP Package.
Unfortunately I can not work with BGA :-(
hi
i'm using ADV7611 for Hdmi input, RGB 888 output.
i have some question.
Q1. I was send to ADV7611 {0x98, 0xFF, 0x80 } for reset i2C. but i can't receive ack from ADV7611.
other setting, received.. why ??
Q2. my configuration this.. is…
电子电路百科全书6-8/8
We have connected a parallel digital to analog converter to the data bus and we are using the AMI to access it. Our AMI setup is as follows:
*pAMICTL3 = ( AMIEN | BW16 | PKDIS | WS5 | HC2 | AMIFLSH | PREDIS);
We have noticed that the lower 8 bits…
AD7124-8设计用于8路T型热电偶测温电路,冷结补偿使用ADT7320,基准使用ADR4525,通过隔离电源和数字隔离芯片实现与后端MCU的隔离,隔离电源使用ADUM6028+ADP7118-33,数字隔离芯片使用ADUM251N1。该设计参考AD7124-8的ADI实验室电路,在测试过程中发现一个问题,当大于2路以上的热电偶同时放置于盛有自来水的水杯中时,发现AD7124-8测得的温度出现跳变,跳变出现在热电偶测温端(热端)同时放入水中时,此时温度跳变较剧烈,放入水中5~10秒后,跳变结束…
Hello,
I am using AD 9364 no-os API to configure the TX LO fastlock switching mode. For a less than 8 number of frequency, i am able to configure successfully using store and recall apis but not able to configure properly for more than 8 frequencies.…
we use the LTC4162 battery charger in several projects, both with Lead-acid batteries and with Li-ion batteries.We would like to use it also in a new project with a 8-cells Li-ion battery pack.
My concerns regards the full-charge battery voltage…
I am using the ADF4360-8 to as an input to my IQ receiver which divides the vco frequency by 2. I use a reference frequency of 19.2MHz, an Fpfd of 50kHz and tune the VCO to 300.050MHz (count 6001) and I get these spurs on my ground at 150.000MHz and 150…