Hi,our customer found that AD9914 usually work well and unlock under +85℃.Can you help to analyze reason?
Datasheet contents information about vertical lock range. It is limited by 70 Hz. But maximum sample rate is 170 MHz. Could ADV7441A support resolutions (from RGB source) up to 1280х1024 @ 85 Hz?
Hi there
Datasheet of ADG719 (p. 4) does not give any indication regarding Idd at high temperatures (e.g. 85 deg C) or maximum rating over operating temperature range. Only value at room temperature is given. Could this be specified?
Many thanks.
Hi Folks,
I've got a customer who wants to do 8 bit A-D conversion on an RGB channel. His ideal part would be if the AD9984A was spec'd to run at -40 to +85 deg C. We have some parts that do this, although many of them are overkill with HDMI interfaces…
ADG884 switching issue at 80-85 Deg. C operating temperature.
We are using ADG884 in data acquisition system.
ADG884 is multiplexing two difference voltage followed by instrumentation amplifier and Delta sigma ADC. The 1st voltage is 25~50mV and 2nd…
Hello,
For a card featuring multiple AD5755-1 and ADAS3022 converter as well as OPAMPs, I'm looking for a 5V In to +15V 350mA Out analog power supply solution (operating temperature up to 85 deg. C, air cooled) (low ripple)
Any proven/verified/recommended…
ADIS16460,According to datasheet, Operating temperature range: −25°C to +85°C,why some showing -10°C when we test?
[#6891] traps test may fail at case 85 'Read of L1 instruction' on bf518f-ezbrd in 2011r1
Submitted By: Vivi Li
Open Date
2011-11-21 03:06:15
Priority:
Medium Assignee:
Nobody
Status:
Open Fixed In Release:
N/A
Found In Release:
Hi Steven,
I don't see where vBootTask is created twice. What make you think that?
there is 2 task that seem created: prvIdleTask and vBootTask. Could you point me where you see that vBootTask is called several time?
If you look at where the context…