• LTC1685 IBIS model

    Hi!

    I like to implement a serie resistor on RO output signal (pin 1) when using 50R transmission lines for good signal integrity. Hence the following questions:

    1. Is there any IBIS model available to the LTC1685 transceiver?

    2. What is the approximate…

  • LTC1685 ESD

    Hi!

    I use a LTC1685 transceiver pair in an application. To protect the input/output A and B pins of the LTC1685 I use a common mode chocke and TVS diode CDSOT23-SM712. However, the capacitance of the TVS diode is 75pF and the system fail to transmit…

  • LTC1685 fail safe

    Hi!

    The LTC1685 RS485 transceiver have fail-safe feature according do the datasheet.

    According to your application note AN-960, the fail-safe mode is working because -30mV or more is detected as 1. and less then -0.2V is detected as 0. (However, the…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • SPICE model for LTC490 (differential driver and receiver pair)

    Hi,

    Is there a SPICE model for LTC490 differential driver and receiver pair? If not, is there any other way to simulate this device in LTSPICE?

    I need to perform simulations in order to find an issue in a circuit that is using this device, but I have…

  • 【在线研讨会讲义下载】了解ADI高性能隔离器解决方案,这个文档就够啦

    近日,ADI 在电子发烧友官网举办了一场在线研讨会【ADI 创新的高性能隔离器解决方案】,向大家展示了 ADI 面向以下应用示例的接口和隔离产品组合:

    • 适合军事和航空航天应用:隔离式 RS-485 收发器

    • 适合高速背板扩展和模拟前端:隔离式 LVDS 产品

    • 适合工业或测试测量系统:隔离式 总线

    • 高度互补的产品组合开创行业最全面的高性能隔离式通信产品套件

    点击链接;http://webinar.elecfans.com/393.html?elecfans_trackid…

  • 官方资料上线丨《数字隔离和接口技术选型指南2021》免费下载ing~

    “数字化”正在全球范围内掀起浪潮,推动科技如闪电般速度发展:数字医疗健康、电动汽车、 5G通信和智能制造……
    电子化器件中离不开隔离技术,而数字隔离凭借其更低的噪声和电磁干扰、更高的安全性以及更长的使用寿命,是隔离发展的必然趋势。
    ADI在数字隔离技术方面有着丰富的经验,iCoupler数字隔离可保护人员和财产免受高压影响,并保护关键数据免受破坏性电干扰。
    那么面对不同的应用领域,如何选择适合的数字隔离和接口解决方案以最大化加速您的项目?

    AD…