• RE: HMC666_using IF pin without 1:1 transformer

    Hi Josh,

    IF port could be used as single ended but the conversion loss will be 3dB more than specified in datasheet, and the isolation maybe worse.

    Regards.

  • AD8195:  1:1 HDMI/DVI Buffer with Equalization

    Is there any documentation for the evaluation board for the AD8195?

    Thanks,
    John

  • Powerful Combinations are Possible when 1+1>2

    It’s a new beginning for Analog Devices and Linear Technology. Together we become the high-performance analog industry leader with an innovation engine fueled by our comprehensive portfolio of analog and mixed signal products and solutions.

    We have…

  • What the difference between the ADA4940-1 and the ADA4941-1?

    What is the difference between the ADA4940-1 and the ADA4941-1? They are both ADC drivers, but what distinguishes the two parts from each other?

  • How to configure 1 TX-1 RX in No-OS

    Hi all,

        My design uses ADFMCOMMS2 module and ZEDBOARD, I want to transmit data using 1 TX- 1 RX but the default set 2  TX-2RX in No-OS, so what parameters in  default_init_param in main.c file I need to modify in order to  set 1 TX- 1 RX, thank you for…

  • ADA4627-1 and ADA4637-1 Null Inputs Connection

    Hi,

    ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?

    Regards,

    Ivan.

  • ADF7030-1

    Hello,

    I bought the ADF70301 - 433 EZKIT and I can't find, in the ADF70301 data sheet, the noise figure of the transceiver. 

    So I'm here to ask: how can i measure the noise figure of the ADF70301 using the 433EZKIT?

    Thank you for your support

  • ad7656-1

    I'm requesting the gerber files for this product mentioned above... is it possible to receive them. thanks, 

  • LTC2439-1

    Hi!

    We wanna use the LTC2439-1 configured with 16-Channel Single-Ended Inputs, the Reference-Voltage is 5.0V and the Input-Channel Voltages are from 0-5.0V

    But the datasheet does not clearly describe the function for us with this configuration.

    We are not…

  • ADUM4121-1

    Can ADUM4121-1 gate drive handle 100% duty cycle?