• How to configure 1 TX-1 RX in No-OS

    Hi all,

        My design uses ADFMCOMMS2 module and ZEDBOARD, I want to transmit data using 1 TX- 1 RX but the default set 2  TX-2RX in No-OS, so what parameters in  default_init_param in main.c file I need to modify in order to  set 1 TX- 1 RX, thank you for…

  • LTC2942-1

    Hi.

    The Sense+ pin is connected to both Charger and Load. So,I would like to know how the LTC2942 could determine the operation mode between charge and discharge.

    Thanks.

  • ad7768-1

    Hello,

    I want to use the AD7768-1 with 5V AVDD1 = Vref and 3,3V VDDIO.
    In demo-circuits the AVDD2 is connected to probably noisy VDDIO!
    Wouldn't it be better to supply AVDD2 from 5V over a R-C-Filter, that would lower the voltage to around 3V?

    Additionally…

  • ADA4941-1

    Hi All,
    I am looking for OPAMP which can convert single ended signal to differential signal to drive the ADC which has differential input. I have selected ADA4941-1 and tested for -2 and +2 gain configurations which are mentioned in Figure 58 and Figure…
  • ADF7030-1

    Hello,

    I bought the ADF70301 - 433 EZKIT and I can't find, in the ADF70301 data sheet, the noise figure of the transceiver. 

    So I'm here to ask: how can i measure the noise figure of the ADF70301 using the 433EZKIT?

    Thank you for your support

  • LTC2439-1

    Hi!

    We wanna use the LTC2439-1 configured with 16-Channel Single-Ended Inputs, the Reference-Voltage is 5.0V and the Input-Channel Voltages are from 0-5.0V

    But the datasheet does not clearly describe the function for us with this configuration.

    We are not…

  • ADUM4121-1

    Can ADUM4121-1 gate drive handle 100% duty cycle?

  • AD7988 - 1

    Good afternoon....

    I currently am using the above subject successfully in a design.  The power supplies are as follows: Vref = 2.5V, VDD = 2.5V and VIO = 2.7V - 3.6V.  Moving forward I would like to re-route the analog supply, VDD to track with VIO.  Can…

  • ad7656-1

    I'm requesting the gerber files for this product mentioned above... is it possible to receive them. thanks, 

  • ADF7030-1

    Dear Sir,

    How to test the receiver sensitivity in ADF7030-1 eval board?