• Ad4360-7 phase noise

    Dear sir ,

    I want to use Ad4360-7 fo generate a local oscillator at 1500Mhz for a gps rx. Ad4360-7 draws about 37mA at 3.3 v  about 100mW, but the phase noise is poor. Ad3450 is much better but it draws over 500mW. Far too  much for my restrictions. Could…

  • AD9361 Artix-7 drivers

    Hi,

    Can you give some information of Artix-7 AD9361 API Drivers.

    Regards,

    Ravi

  • ADF4360-7 VCO drift

    I am looking for the drift of the VCO  in the ADF4360-7.  I understand that the output of the VCO is ± 3 dB Typ over the full temperature range is discussed here:

    https://ez.analog.com/message/86637#86637

    I am looking for how the frequency changes with…

  • ADF4360-7 Not locking


    Hello

    I have a design that uses a 4360-7 and I am unable to get it to lock. I have used ADsim to generate the parameters for a 1GHz output frequency. I have the R counter set to 2 which gives a 5MHz PFD frequency from a 10MHz ref clock. I have validated…

  • AD7366/7 AGND & DGND

    Dear all,

    If the hardware that we will be working on only have one GND, can the AGND and DGND be shorted together? Or it should have separate ground panels? Will there be any issues if its combined? 

    Thank you.

  • ADF4360-7 Single-Ended Output


    Hi,

    Is it possible to have a single-ended RF output from ADF4360-7.
    If it is possible, is it just enough to connect unused RF output pin to ground via a 50 ohm resistor or should I use a balun ?

    Thanks in advance.

  • HMC746 FPGA kintex 7 xc7k325t_900

    How should the CML level standard IO pin of HMC746 be connected with FPGA

  • RE: Upgrade from ADAU1701 to 6 or 7 stereo I2S inputs

    Hello Benno,

    So you need one I2S, and either two TDM4 or one TDM8 inputs. Your earlier post made it seem like you needed 6 or 7 I2S lines which cannot be done with the ADAU452. It can only do four I2S inputs. It can also do 4 TDM inputs so it can certainly…

  • ADP5033ACBZ-7-R7 SPEC temperature

    I didn't found.

    Could you provide me the unit chip temperature and resistance?

    Thx!

    P/N:ADP5033ACBZ-7-R7

    1.θ

    2.θja  

    3.θjc

    4.θca

    5.TC,

    6.TJ,

    7.TA

     

  • ADSim - Windows 7 64 bit

    Hello.

    A colleague of mine asked me, to find a way to run “ADSim” on a Windows 7 (64bit) system.

    It seems to be working fine on a Windows 7 32bit system.

    Is there a supported way on a Windows 7 64 bit? Is there a successor of this pretty old version…