• LTC1164

    I am trying to use the LTC1164 for notch filtering but I'm just not sure where to learn how. I've gone through the datasheet and set all the pins as necessary but the filtering just does not work. If anyone knows any materials I could use apart from the…

  • ADF4360-7 Evaluation Board Software for Windows 7

    Hello,

    I tried to install the ADF4360_V301 and also ADF4360_v2_0 on windows 7 32-Bit.

    both of them failed to run:

    V2_0 showed Run-time error '53': File not found: parllio

    I guess the printer port for the serial connection can not be initialized…

  • cp_vid_std[7:0] (IO Map, Address 0x05[7:0]) of ADV7480.

    Hello,

    I have questions about register cp_vid_std[7:0] (IO Map, Address 0x05[7:0]) of ADV7480.

    We think we don't have to change cp_vid_std according to HDMI input resolution.

    Your S/W driver(SRC-Rel1.5.0_BETA) seems to set cp_vid_std to "0x53"…

  • RE: AD9697 and Kintex 7 SYNC problem

    please refer to DETERMINISTIC LATENCY and MULTICHIP SYNCHRONIZATION sections of the datasheet. the sysref frequency should be an integer divider of internal LMFC

  • [ADV7280A] Saturation register (SD_SAT_Cb[7:0] (Address 0xE3) and SD_SAT_Cr[7:0] (Address 0xE4))

    Hi,

    I have a question about saturation register (SD_SAT_Cb[7:0] (Address 0xE3) and SD_SAT_Cr[7:0] (Address 0xE4)) of ADV7280A.

    The table 27 and table 28 on UG-1176.pdf shows as follows:
    0x80 Gain on Cb channel = 0 dB
    0x00 Gain on Cb channel = −42 dB…

  • RE: AD9697 and Kintex 7 JESD connection problem

    if the ADC's JESD204B pll is locked, then the issue most likely is on the fpga side

  • RE: Regarding REF_MUX_CTRL[7:6] bitfield for Internal reference on EVAL-AD7779FMCZ(AD7779)

    Hi, 

    Apologies for missing this item. But to answer this query. You can use either of the two settings. The figure 98 you mentioned, is a suggested way to connect the internal reference to the external reference's input (but remember to configure the ADC…

  • Amplifier LTC6019-7 related problem 咨询关于LTC6019-7这款程控放大器的问题

    LTC6910在单5V供电工作状态下,其输入时钟可否大于3MHZ,或者说在单5V供电的工作状态下,其-3dB截止频率可否高于150HZCan the input clock of LTC6910 be greater than 3MHZ under the single 5V power supply working condition, or can the -3db cut-off frequency be higher than 150HZ under the single 5V power…

  • some problems about filter,LTC1069-7,thanks,关于滤波器1069-7的一些问题,万分感谢

    Can the input clock of LTC1069-7 be greater than 3MHZ under the single 5V power supply working condition? or can the -3db cut-off frequency be higher than 150HZ under the single 5V power supply working condition?
    LTC1069-7在单5V供电工作状态下,其输入时钟可否大于3MHZ,或者说在单5V供电的工作状态下…
  • ADF4360-7.

    HI, I am using several of the Eval boards for ADF4360-7. I use the Eval software. I have never gotten a lock light after trying several different frequencies including the center of 900Mhz. I notice I do get a full power output after selecting "Mute until…