• RE: LT8711 - Buck-Boost mode

    Has the LT8711 model been fixed? as I am simulation a Buck-boost and I want to make sure everything is good

  • LT8711 SEPIC Converter BIAS and IntVEE pins

    Hi everyone,

    We are designing a power supply using the LT8711 in SEPIC configuration..

    Regarding the datasheet, it specifies to connect INTVee to BIAS pin:

    In the demo board schematic DC2234A it is connected as the datasheet.

    On the other side, in…

  • LT8711

    Hi I am confused with the explanation regarding some of the calculations for the Boost topology on page 15 of the data sheet for the LT8711.
    Please walk me through the step  2 and  3 .  Also  please define for me the units of DC max  and how it relates to the…

  • LT8711 LTSpice model issue

    Is this a bug in the LT8711 LTSpice model, or have I set it up incorrectly?
    The LT8711 is hiccuping because the IntVcc pin is hitting its UVLO threshold (3.9V). The current into the pin is spiking between 200 and 400mA while the circuit is switching, and…

  • RE: Question of LT3942

    Hi

    For higher output current capabilities, I would suggest looking on LT8711, LT8390A, LT8390 or LT3790.

    If you are looking for a more compact solution you could look on to LTM8054/5 or LTM4605

     Regards, 

  • sychronous SEPIC converter

    Hi there,

     

    I am looking for sychronous SEPIC converter controller IC. Input voltage 8~16V, and output 20V 1A. I found LT8711 which is for one PMOS and one NMOS. Do you have any power management IC with two NMOS driver in SEPIC converter application? Or…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032