• RE: LT8711 - Buck-Boost mode

    Has the LT8711 model been fixed? as I am simulation a Buck-boost and I want to make sure everything is good

  • LT8711 SEPIC Converter BIAS and IntVEE pins

    Hi everyone,

    We are designing a power supply using the LT8711 in SEPIC configuration..

    Regarding the datasheet, it specifies to connect INTVee to BIAS pin:

    In the demo board schematic DC2234A it is connected as the datasheet.

    On the other side, in…

  • lt8711能否通过外接实现同步整流?

    如题,如果能实现的话 需要怎么接

  • LT8711

    Hi I am confused with the explanation regarding some of the calculations for the Boost topology on page 15 of the data sheet for the LT8711.
    Please walk me through the step  2 and  3 .  Also  please define for me the units of DC max  and how it relates to the…

  • RE: LT8711 LTSpice model issue

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 矿业级产品使用DC-DC咨询

    目前本安电源项目使用的DC-DC,对于输入输出电容要求很严苛,推荐一款产品一下。

  • RE: synchronous SEPIC Converter

    您好,有关LT8711的使用问题 请在咱们英文社区提问哦ez.analog.com/search

  • RE: Question of LT3942

    Hi

    For higher output current capabilities, I would suggest looking on LT8711, LT8390A, LT8390 or LT3790.

    If you are looking for a more compact solution you could look on to LTM8054/5 or LTM4605

     Regards, 

  • sychronous SEPIC converter

    Hi there,

     

    I am looking for sychronous SEPIC converter controller IC. Input voltage 8~16V, and output 20V 1A. I found LT8711 which is for one PMOS and one NMOS. Do you have any power management IC with two NMOS driver in SEPIC converter application? Or…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032