Hi all,
I want to know, if I can get negative voltage (-48 V) with output current 5 A from LT8710 (LT8710EFE#PBF)?
Input voltage is between +16 V to +33 V
Thank you very much for answers.
Regards
Vojta Kana
Hi all,
I want to know, if I can get negative voltage (-48 V) with output current 5 A from LT8710 (LT8710EFE#PBF)?
Input voltage is between +16 V to +33 V
Thank you very much for answers.
Regards
Vojta Kana
I am designing a Synchronous SEPIC, but I need A5 amp gain that is connected to Rsense1 in order to obtain Rf and implement mi compensator.
I am designing an asyncronous boost converter using LT8710 with a requrement of input current limiting.
The idea is to use a current sense resistor connected to ISP and ISN pins. As TG drive is not required for the asyncronous design pins INTVee and BIAS…
Hello,
our LT8710 is a controller for SEPIC topology (beside others) which features possible output current control:
https://www.analog.com/en/products/lt8710.html.
One of the examples:
kind regards
Markus
Dear Sir or Madam,
I'm looking for a SEPIC Controller with 1 MHz Switching Frequency and a max. Output Voltage of 400 V. The max. Output Power should be 100W. So I will have a Input Voltage of 100V by 2A.
Is it possible to use the LT8710 to get the…
So you need a boost converter that can regulate the output voltage (CV mode) at 60V and regulate the output current (CC mode) when the output voltage drops below the programmed value. That limits the part selection greatly and the LT8361 won't be easy to work…
Hi,
I have a question about an application that requires inverted voltage polarity in a test chamber. Please let me explain the application background first, and then ask the question.
[Application background]
In normal mode (i.e. cooling), no voltage…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |