• LT8708 and LT8708-1

  • Can LT8708-1 be used as a standalone DC-DC if not in parallel with LT8708?

    Can LT8708-1 be used as a standalone DC-DC if not in parallel with LT8708? Can LT8708-1 be used independently?Does working alone achieve the same functionality as LT8708?

  • wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    The LT8708EUHG-1#PBF specification shows that the LT8708-1 always operates as a slave to the master LT8708, Mainly used in parallel with LT8708, At present, our customer wants to use LT8708-1 (LT8708EUHG-1#PBF) separately without parallel connection.…

  • LT8708/LT8708-1 More Parallel Output Design

    Dear All:

    The DC2719A is LT8708*1 + LT8708-1 *1 design solution ,If I need LT8708*1 + LT8708-1 *N The Output component how to placement ,my product estimate use LT8708 *1 + LT8708-1 *4 pcs parallel output ,the MOSFET ,capacitance...etc component ,have…

  • LT8708 can't soft startup recover when it's enter to overcurrent state!!!!

    Dear teams: 

        I just use lt8708 for double battery applications, Now i just test And find some problem as following:

    1. In input i just use a 10A 48V power supply(PS)

    2. In Output, a Electronic load for test the LT8708's efficient

    3. Setting the IMON_OP…

  • LT8708 for regenerative braking

    Hi, 

    I'm currently designing an application where I have a 12V battery that powers a 24V motor. My motor can sometime gain energy in the field and its voltage can rise up to 40V. During this voltage rise, I'd like to use this motor energy to charge my…

  • LT8708 is only used in the depressor mode. How do I deal with the BG2,BOOST2,SW2,TG2 and pins of LT8708?

    LT8708 is only used in the depressor mode. How do I deal with the BG2,BOOST2,SW2,TG2 and pins of LT8708?

    1,Can the switch tubes of 1, M3 and M4 not be used?

    2. Is there a reference schematic for LT8708 to work only in the step-down mode?

    3. The input…

  • Fault of Imon_Op (LT8708)

    I designed battery charger circuit with LT8708. The circuit is working correctly. Imon_INN, Imon_INP and Imon_ON pins also work as described in the datasheet. I'm just having trouble with the Imon_OP pin.  Although my output current increases, the…

  • IMON_OP fault of LT8708

    Hi,

    I designed Battery Charger with LT8708.  When ı run the circuit, circuit is protected and doesnt work. Because Imon_op pin reaches 1.22 V. Why is pin Imon_op 1.2 volts when the circuit is not working?


  • LT8708 LTSpice model

    Hello,

    I look for LTSpice model or circuit model(demo) for LT8708, is there please any one available from AD?

    Thanks,


    Fernando Romano.