• LT8641 VS. LT8643S

    HEY ALL,

    i'm designing a new board and considering using one of those parts: LT8641 / LT8643S

    wanted to know if someone can share from his experience regarding.

    as i know, the LT8643S is newer part, silent switcher 2 , which i cannot tell the difference…

  • RE: LT8643S DC-DC converter Enable by Switch/MCU

    Hi, 

    I think you can implement this with an AND gate using a combination of FETs. Can you share your schematic?

    Regards. 

    Fritz

  • a question regarding LT8643 output voltage ramp rate

    Hi

    Here is a question regarding LT8643 output voltage ramp rate, the schematic diagramwhich I used as below. The SS capatior I used is 0.1uF, Now I test the output voltage rising  time is 50ms which is so slow for me.I would like to get faster rising time…

  • Clock distribution to 2 DDSs (9913) and 2 ADCs (AD7769)

    Hi,

    I am goning to distribute a common 40 MHz clock to 2 DDSs and 2 ADCs. Will AD9577 work for this purpose? If not, do you have any suggestion?

    The ADC needs 5 V CLK and the DDS needs 1.8 V CLK.  

  • JPEG Processing - 4:2:2 v 4:2:0?

    My JPEG saga continue...

    I am using a BF561 single core to compress a 640x480 YUV 4:2:2 image into JPEG format, employing the ADI JPEG Library tools.  I am getting very poor performance compared with the reference results from the Spec Sheet.  The Spec…

  • ADV7842 4:2:2 DDR mode, ADV7393: Stanag3350 support?  (2)

    Hello Dave,

    I am facing problems with replies to your answer, so I am oppening a new dicussion with the same title.

    Please clarify your answer regarding STANAG support:

    2) As I understand it, this is the same as RS-343A/EIA-343A and none of our parts…

  • LTC6804-2 and LTC6811-2 reference voltage 1 and 2 at 0V.

    Hello,

    I installed 2x LTC6811-2 and then 1x LTC6804-2 on the same board and I don't have any voltage reference output at anytime. The functional diagram in the datasheets shows that VREF1 should be always present as it's generated from V+. VREF2 is not…

  • 2*2 MIMO setup

    Hello,

    Iam interested in implementing a MIMO 2*2 scenario where i will use 2 fpgas (1 as the transmitter and 1 as the receiver) where each one  will be connected with one AD-FMCOMMS3-EBZ.
    So the setup will be :
    FPGA_1 + AD-FMCOMMS3-EBZ_1 =Base stati…

  • ADV7403 YUV 4:2:2?

    Can the ADV7403 output YUV 4:2:2 rather than YCbCr 4:2:2?

    Thanks.

    Chris

  • 4:2:2 8bit ycrcb

    Hi,

    I have the EVAL-ADV7612-7511p video evaluation board .I'm using 7612 to receive  HDMI inputs from camera(720p @60) , and then feed to 7511 to output the video to the screen. 

    camera -> 7612 --> 7511 --> screen

    When adv7612 output 4:4:4 8bit ycrcb…