• RE: LT8610AH/LT8610ABH thermal shut-down

    Hello,

    Thanks for application of LT8610 products. 

    Yes, LT8610AH/LT8610ABH have on-chip thermal-shutdown feature.

    The threshold is around 165C degree.

    Best regards,

    Andrew

  • LT8620 stability using LT Power CAD

    Hi All,

    We are using LT8620 to generate 1.2V from 7.5V. We have very wide output load variation from 10mA load to 2A load. So, I would like to understand stability of the circuit that we designed under different loading conditions. Unfortunately, LT8620…

  • RE: LTPowerCAD crash when opening file

    I was unable to reproduce the error. Including changing windows region and language settings for France those default solutions mentioned seemed to load without error. Can you send an image of the error message shown when you try to open the default solution…

  • AEC-Q100 for LT / ADP

    Hi,

    I am currently looking into the part like LT8610 & ADP1612.

    We found most LT components has automotive temperature "H" grade selection.

    However, we does not find any info regarding to AEC-Q100.

    Does "H" grade represent the AEC-Q100…

  • RE: LT8610AC In parallel or in the same board

    HI, thanks for suggestion. I saw LT8650S as well as LT8645/46. I decided to use LT8610 because according to LTSpice simulations it lead to a small ripple (even in the range of 1 mV by proper selection of output capacitor and inductors) and in nominal…

  • 【在线研讨会】Silent Switcher稳压器: 高效率、超低EMI

    在重视热耗散和效率的场合中,人们会用开关稳压器替代线性稳压器。开关稳压器通常是输入电源总线线路上的首个有源组件,因此对于整个转换器电路的 EMI 性能具有重大的影响。

    EMI发射有两类:传导和辐射。传导发射通过电线和走线连接到产品。辐射发射测试只有在设计基本完成之后才能正式进行。

    在近期的在线研讨会《Silent Switcher稳压器:高效率、超低EMI》中,从原理到封装到布局再到具体产品,重点介绍了大幅降低开关稳压器EMI辐射的新技术。

    首先,高频噪声来自哪里?在电子电路中,通过寄生电阻…

  • RE: 能获ADI&世健万元大奖的电源设计,究竟长什么样?(内有福利哦~)

    ADI & 世健·电源智造设计赛 三等奖

    基于 ADI- LT8610 的高效 2.5V 电源轨

    Black small square 输入电压12V, 输出电压2.5V,持续输出电流能力不小于2A;

    Black small square 整版使用电容合计容量,不得大于60uF;

    Black small square PCB 仅限于2-4层,不接受6层及以上PCB设计。

    选型工具使用 ADI 的 LTpowerCAD II,现在的设计辅助工具可以帮助工程师节省很多的时间,个人非常推荐学习和使用,还能避免一些人为错误,大大降低了设计难度,缩短了研发的周期。

    ADI & 世健·电源智造设计赛…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032