• LT8609S Output Voltage Range

    Hello,

    Could you please let me know the output voltage range of LT8609S?

    Generally, the output voltage range is specified in the datasheet, but for the LT8609S, I can't find it.

    In the case of LT8609S, after calculating the on-time using the input…

  • LT8609

    What is the current consumption of the LT8609, Sync tied low, when out of regulation. I am using the device as a voltage limiter, Vin is 11 to 30V, Vout set to 12V. 10uH 3 amp inductor. I am finding it draws around 2mA when Vin is less than 12V

  • RE: Maximum Vout of LT8609S

    Hello,

    the maximum VOUT of LT8609S is just a function of VIN and can be differenciated for the two operating modes:

    1. Dropout. Please check these two diagrams from the datasheet:

    2. In 'regular' operation the maximum duytcycle (dependent on frequency…

  • RE: Can I replace COILCRAFT XAL4020-222ME with Wurth Elektronic 74438366022? LT8609

    Hi vengineer,

    The Wurth inductor looks ok. I did quick comparison of two specs: ISAT, IDC specs of Wurth are good. This inductor is slightly bigger though. 

  • LT8609 - Automotive package

    Hello,

    I plan to use LT8609 for automotive application.

    What is the better package between DFN and MSOP for this usage?

    I mean about robustness.

    Usually, is the smaller the better?

    Best regards,

    Martial

  • LT8609 EN Input Restrictions?

    Are there any restrictions on the LT8609 relative to Vin?  For example, can EN be set high by logic prior to Vin turning on (ie. Vin is zero or below EN threshold (below ~1.05V) and EN is >3Vdc)

  • LT8609S Sub-harmonic oscillation

    Looking at the LT8609S as a pre-regulator outputing 6.3vdc @ 1.2 Amps.
    Working through the datasheet it appears that a 22uH inductor at 400 kHz
    is reasonable. I'd like to support an input range from say 9v to 12v
    meaning duty cycles greater than 50%…

  • LT8609S Ultra-low EMI

    Hi Analog,

    Could you provide me with the right ferrite bead that I could use in this schematic or a way to determine it myself:

    www.analog.com/.../LT8609S.pdf

    Ultralow EMI 3.3V 2A Step-Down Converter

  • is there any Bug in LT8609 spice model?

    Hi all

    i do a simulation with LT8609. but there is some big spike noise about 10Vp-p on Vin, when Cin has 0.6nH of ESL.

    and , there is no problem in LT8609A  with same simulation.

    is there any Bug in LT8609 spice model?

    Best ragards

  • LT8609S ext clock using LTC6902 with SSFM

    Looking to drive three LT8609S regulators from a LTC6902 with SSFM.  This appears fairly straight forward ... float DIV and PH (each bypassed with a 1nF capacitor), 10.5K SET for a 630kHz Fmax, 22K MOD for a 9.55% SSFM.  Connect OUT1 to the first LT8609S…