• LT8602 cant download LTpowerCAD file

    High voltage cant download,show there is a network error.

  • LT8602 Iq higher than expected.

    Hi,

    I have the following circuit using the LT8602 for power distribution and rudimentary SLA charging.   In the configuration below, I am seeing 2mA quiescent. current  with only the PVin2 source attached, (no PVin1 has no source)

    PVin1 is the input for…

  • LT8602 and LTspice

    Hi all.

    I'm simulating the LT8602 with LTspiceXVII.

    The four outputs are: OUT1=5V, OUT2=3.3V, OUT3=1V and OUT4=1.8V

    I'd like to have the follow startup sequence: OUT1 -> OUT3 -> OUT4 -> OUT2 

    For OUT1, OUT3 and OUT4 there are not problems…

  • LT8602 and FPGA

    I'd like to use LT8602 to power FPGA like XILINX SPARTAN7 because it is possible to generate 4 different voltages in sequence and because in my board the input voltage is 24V.

    The 4 currents requested from my FPGA are under 1A and so I think that…

  • Output capacitor for LT8602

    Hi all.

    From the LT8602 datasheet, pag. 19, I saw that the output capacitor should be: Cout>10*L*(Ilim/Vout)^2.

    For channel 3 and 4, is the Ilim(TYP) = 3.1A?  (In the datasheet pg. 4-5 I saw SWx Average current limit between 1.8-3.5A).

    If so, with…

  • RE: LT3507 Input range

    Hello,

    even if LT3507 can do the job (which I have not evaluated completely) our newer parts are better in terms of  efficiency, solution size and Vin requirements:

    LTC3644

    LT8601

    LT8602

    ADP5014

    What I cannot judge on right now is the current availability…

  • RE: Lt3504 Output Combination

    Hi,

     

    Thanks for application of LT3504.

    LT3504 is not specially designed for parallel operation. The internal compensation in each channel is independent with each channel having its own duty cycle, so the current balance may not be ideal especially at…

  • RE: LT8602IUJ#PBF top marking request by each line explanation

    Hi Polo,

    Thanks for your interest in LT8602.  It is our company policy to refrain from discussing product marking details in this engineerzone forum.  Please contact your authorized ADI distributor, regional representative or field applications for the…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032