• Modifying Output of DC2345A for 40V, 5.5 A

    Good evening,

    I purchased a DC2345A evaluation board for the LT8391A. I modified the board to output 40V by changing R6 to 25KOhms and 5.5A by modifying the sense resistor to 18 mOhms. This works great when running the LEDs at 100% duty cycle.

    However…

  • RE: driver for led

    Hello lidas,

    I see that you are looking for an LED driver with these specs...

    input voltage from 3v to 18v and a 12v and 2.1A output

    This clearly requires one form or another of a buck-boost topology.

    The LT8391 is a great buck-boost to use (with…

  • parallel LT8930A controller clock synchronization without external clock?

    I would like to parallel two LT8930A controllers and synchronize the oscillators with 180° phase offset. Is it possible to do this without an external clock? If so, how?

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032