• 请教一下 LT8390和LT3790的区别?

    请教一下 LT8390和LT3790的区别?

  • RE: Question of LT3942

    Hi

    For higher output current capabilities, I would suggest looking on LT8711, LT8390A, LT8390 or LT3790.

    If you are looking for a more compact solution you could look on to LTM8054/5 or LTM4605

     Regards, 

  • RE: LT8390 Parallel Function

    Hi 

    Please use the article below as reference:

    https://www.analog.com/en/technical-articles/60v-synchronous-low-emi-buck-boost-for-high-power-and-high-efficiency.html

    Some highlight that could be taken on the article is to tie the IMON pin on the master…

  • About LT8390A output Current?

    Hi,

         I design a power system by using LT8390A, Input Valtage is 9~60V, output voltage is 12V, output current is 15A, here is the schematic, Please help check 

         And I find LT8390A output current is 10A, so Can i use LT8390A in my design?

         And what is…

  • RE: LT8390 chokes while driving motors in Buck mode

    Hi

    The eventual goal is 100 Amps, @ 24Volts using 2 LT8390 boards in parallel. However in the test i preformed, motors stalled before 200 Watts.

    I am trying to regulate the Output voltage

    Load is definitely inductive since it powers motors through…

  • LT8390 Buck-Boost Controller

    Can LT8390 do VIN=18V~50V,Vout=24V/12.5A (300W) by single chip?

    Is there any reference design for the spec?

    Thank you for your help.

  • LT8390 MOSFET design

    Hi Sir

    Consult the LT8390 DC2431A circuit design
    M1 / M5 and M3 / M7 use two, but in M2 and M4 only one?

  • LT8390 LTPowrCAD Result value Question

    Customer : KyungShin 

    Application : Charging of supplementary battery for DVRS

    Remark

      - My customer is designing the schematic and calculating the Power Loss at Current Sensing Resistor

      - when check the LTPowerCAD, They understanded at Power Loss at load…