• LT8316 as a Buck Regulator

    Hello - is there any documentation available for using the LT8316 as a buck regulator?  I am designing a circuit which is very close to the example circuit given in Figure 9 (with an extended VIN input voltage using zener diodes for up to 1000V in), but…

  • Non-isolated LT8316 does not work

    Circuit: www.analog.com/.../lt8316.pdf

    Hi there,

    I have built a circuit based on the datasheet application Figure 9. Nonisolated 24V Buck Converter with Optional Undervoltage Lockout (with modified feedback and components due to availability at our distributors…

  • LT8316 can make 10kV output ?

    Hello,

    I'm looking for a flyback converter to be able to make 10kV/1mA output.

    My target spec is Vin=24Vdc, Vout=10kV, Iout=1mA max and my product is capacitor board to replace vacuum capacitors regularly used in

    manufacturing semiconductors.

    Using…

  • LT8316 trouble with mosfet gate drive

    Afternoon,

    I have been prototyping a SMPS using an LT8316 chip. I have had this sucessfully working on a previous revision, but am currently having issues with the gate drive to the mosfet on this latest version. The only changes between the two was…

  • LT8316 Wide Input Flyback Converter

    Hi,

    I am working on a wide input flyback design utilizing LT8316. The Input voltage range should be 18 - 420 VDC and output is 24 VDC @ 2 Amps. In accordance with datasheet, I calculated a transformer with Lpri=180 uH and 4:1 ratio. Since the simulation…

  • LT8316 with 325 Vdc / 3kVA output

    Hello,

    i want to create a power supply with 325 Vdc / 3 kVA out of 565 Vdc Input voltage. Is it possible to create this design with an  LT8316?

    Kind regards Ralf

  • LT8312 or LT8316 using GaN FET

    is there any boundary mode chip design like LT8312 or lT8316 using GaN FET? is there any design example had used it ?

  • Ask a question about LT8316

    Hi,

    There is a similar design as beow, input voltage range is from DC 150V to 400V,the expected output power is 14V/200mA.The used transfomer turn ratio is 10:1,and the inductance of the primary side is 4mH.But this circuit can't work correctly.If the…

  • LT8316 trouble with mosfet gate drive?

    I have been prototyping a SMPS using an LT8316 chip. I have had this sucessfully working on a previous revision, but am currently having issues with the gate drive to the mosfet on this latest version. The only changes between the two was the introduction…

  • About the impulse withstand voltage of LT8316

    Hi,

    I have a question.

    Please give me an answer.

    I want to use LT8316.

    I checked the data sheet, but there was no mention of impulse tolerance.

    There is a possibility that a voltage higher than the rated voltage of LT8316 will be applied instantaneously…