Dear support,
I would like to measure the feedback loop of LT8316 circuit. The documentation doesn`t provide too much details about compensation and loop measurement.
I have tried to measure the loop response with a traditional method, by injecting a…
https://ez.analog.com/power/f/q-a/118175/lt8316-ic-s-24-2a-output-design-spread-sheet-required--reg
Hello Guys,
Need schematic for 20v to 220v input and 12v 3amp output power supply using LT8316
Hi All,
I have a simulated buck converter using LT8316 in the LTspice environment. Although the circuit similar to what shown in picture 7 of datasheet the results are weird. Has anybody this circuit simulated? It seems the chip has no control over output…
Please consider using a clamping circuit to limit the Vin pin voltage.
Hello everyone,
I am facing a problem and I hope someone can help me with.
I am student Electrical Engineer, I am trying to build a flyback converter which converts 350 V DC to 12 V DC at 0.125A.
I used the demo circuit made by Analog, see circuit below…
I'm using LT8316 to build a no-opto isolated flyback converter with 12V/3A, the recommended transformers as per the datasheet are Sumida 11328-T078, Sumida 11328-T074, Wurth 750317589, Wurth 750317463, However none of these are available on Digikey.c…
Hi ADIexpert
my coustomer would like to built a DC 110Vin to 12Vout/5A flyback with LT8316
however, the feedback function of all of the reference design in the datasheet and also EVB are based on a 3rd winding topology
since my customer already has a…
Hello - is there any documentation available for using the LT8316 as a buck regulator? I am designing a circuit which is very close to the example circuit given in Figure 9 (with an extended VIN input voltage using zener diodes for up to 1000V in), but…
Afternoon,
I have been prototyping a SMPS using an LT8316 chip. I have had this sucessfully working on a previous revision, but am currently having issues with the gate drive to the mosfet on this latest version. The only changes between the two was…