I can't find LT8312 in LTpowerCAD.
Can you provide LTpowerCAD Design Tool Config File(*.ltpc) for LT8312.
I need to analyze closed loop stability of the converther using LT8312.
Thank you.
Dear,
My customer would like to simulate LT8312 with Pspice, not LT spice.
May I have a spice simulation model of LT8312 ?
Thanks.
I'm working on a 500 V- 90 V adjustable power supply based around the LT8312, so on my way to designing my own version, I made the typical application circuit given on the first page of the data sheet in LT Spice. I'm in a pickle in that it puts out in…
We have a legacy power supply that has to be redesigned from the ground up. The input is 115 Volts, 400 Hz, four wire, three phase Wye connected. The desired output s a single DC voltage to feed downstream DC-DC converters, which will be designed separately…
So if I use LT8312 for 1St stage Boundary Mode PFC Controller PFC
Cooperate with LT8316 Flyback
Can I use This Solution ?
Hi Eric,
I already went through these IC's (LT3798, LT8312, LT8315 & LT8316), among these LT8315 can't be used for my application as it is having an integrated mosfet.
However LT8316 is Primary side regulation based IC due to which, it's transient…
Hi
Can you share LTspice file for lt8315. and lt8312. Kindly suggest a regulator with which this will be possible even if circuit in datasheet is not present.
Regards & Thanks
Bivin George