• LT8310 - 50Vin; 24Vout; 0.5A Reference design or spreadsheet

    Hi,

    as per subject i'm looking for a reference design or spreadsheet to help to design a 50Vin (60 max) to 24Vout; 0.5A isolated power supply using LT8310 (or better). Operating loweer temp is -55°C

    Any suggestion?

    Thanks

  • LT8310

    I need Vout=57V/1.6A by applying input voltage range is 10V to 53V with using LT8310. Can you please suggest a reference design guide?

  • LT8310 ISOLATED Nonsynchronous WITHOUT an Opto

    Hello,

    I need Vout=24V/6A by applying an input voltage of 24V/25A. Please see the attached. I have selected RSET=50K, considering that Duty Cycle is 0.5. However, the compensating duty mode control loop does not work. I have calculated the L1 and CL based…

  • LT8310 compatible for Vout=56V/1.7A ?

    LT8310 compatible for Vout=56V/1.7A ?(I have taken reference from technical articles of LT8310).
    Can we achieve Vout=56V by changing the following components value? 
    R7 resistor 51.6K and set fsw=194KHz other circuit keep as it is like transformer(turn…
  • LT8310 Output voltage is not getting 54V

    I have used below the same circuitry and components for our application except R13 (10K resistor) is not mounted.

    I have used this reference design from the analog technical article document.

     

     

    Below are the observations while the testing.

    We are applying…

  • LT8310 isolated supply

    Hello everyone,

    I am using the LT8310 and the LT4430 for an isolated 12V power supply. Input voltage is 24V. My setup is very similar to the one on page 33 in the datasheet, except for the transformer ratio - here I am using 1:1. With no load applied…

  • LT8310 and LT4430

    Hello everyone,

    I am using the LT8310 and the LT4430 for an isolated 12V power supply. Input voltage is 24V. My setup is very similar to the one on page 33 in the datasheet, except for the transformer ratio - here I am using 1:1. With no load applied…

  • LT8310

    Hi, 
    I want to build a 19V,10A isolated converter with LT8310.
    Is there any recommended design sample?
    How Can I design it?

  • LT8310 Sample Design

    I'm having trouble getting the isolated, non synchronous sample design for the LT8310 to operate correctly. The feedback seems to have no effect on the operation of the controller. Has anyone had success with this design?

  • LT8310 compensation

    Hello everyone,

    My question is about compensating the circuit in a non-isolated application with current and voltage feedback, exactly in the configuration shown in Fig. 7 on page 22 of the datasheet:

    https://www.analog.com/media/en/technical-documentation…