• LT8300 / LT8303 switching frequency

    Hi,

    Can you provide the mathematical formula allowing to calculate the actual switching frequency of the LT8300 or LT8303 Flyback controllers, depending on the load current, input voltage and output voltage (with parameters as primary inductance, transformer…

  • RE: LT8300 12-50Vin to 5V 1W output

    LT8303 is pin-to-pin compatible.

  • Circuit design on LT3001

    Hello, dear colleagues!

    To clarify: my customer wants to design isolated power supply on flyback converter LT3001 (electrical principal scheme in attachment, transformer is 744889020330 by Wurth Elektronik), he made a board according to this scheme. He…

  • RE: Enquiry related LTC4271/ LTC4290 PSE controller

    Hi Pallavi,

    The C-grade is an IEEE 802.3af, or IEEE 802.3at Type 1 PSE sources 15.4W per port. So your calculation should be 5 x 15.4W = 77W. If your 48V regulated supply is isolated, as are most AC to DC converters, then you can power the LTC4290 directly…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • 寻求技术支持

    大家有用过LT8315EFE的吗?现在我遇到一个问题,就是这个芯片的器件手册里第一页的典型应用电路中的变压器型号没有提供,而且手册中其他应用电路中的变压器型号并没有找到售货商,所以希望有人可以帮我找一下这个变压器的货源和型号。

      PDF

  • 官方资料上线丨《数字隔离和接口技术选型指南2021》免费下载ing~

    “数字化”正在全球范围内掀起浪潮,推动科技如闪电般速度发展:数字医疗健康、电动汽车、 5G通信和智能制造……
    电子化器件中离不开隔离技术,而数字隔离凭借其更低的噪声和电磁干扰、更高的安全性以及更长的使用寿命,是隔离发展的必然趋势。
    ADI在数字隔离技术方面有着丰富的经验,iCoupler数字隔离可保护人员和财产免受高压影响,并保护关键数据免受破坏性电干扰。
    那么面对不同的应用领域,如何选择适合的数字隔离和接口解决方案以最大化加速您的项目?

    AD…