• Reference circuit capable of producing 100W with LT8253

    Hi all,

    I am thinking of modifying an LT8253 evaluation board so that it can output 100W (20V/5A).
    If you have any reference circuits, please let me know.

    Also, the CCG3PA firmware for the DC3004A only supports up to 60W.
    Where can I get a firmware that…

  • DC2949A/DC3004A Maximum Vin

    The user manuals state the max Vin is 18V for both dev kits.  Is there a way to increase the max Vin?  Why is the set to 18V since the LT8253 has a max Vin of 40V?

  • RE: PMIC

    Hi Akshay V,

    I can recommend a 4-switch buck-boost that is actually designed for USB PD specifications. You can check our LT8253/LT8253A which is a Type-C PD PMIC that can handle up to 100W with compliance for USB PD specifications with your own chosen…