• Using LT6658 as a negative reference

    Hi, I would lige to use the dual tracking (posative) referenc LT6658 as a negative reference by connecting its vins and gnd pins to 0v and a negative rail.

    I assume this will work in principal but it's the effect on its noise and stabilty I would be interested…

  • LT6658如何能同时输出正负2.5V的电压?

    LT6658如何能同时输出正负2.5V的电压?,谢谢大神讲解下!

  • 如何用LT6658产生一个0v可驱动大电容负载的电压。

    如何用LT6658产生一个0v可驱动大电容负载的电压。

  • How to use LT6658 to ger a 0v voltage with enough power to drive a big cap like 47uf?

    I 'd like to get a 6v and 0v with big cap loads both load is 47uf. I am looking for a way to get the 0v

  • RE: AD7980 Ref Input Driven by AD780

    Dear Tyler,

    Thank you for your very informative reply. I went thru the article by Alan Walsh that you referred. It was also very helpful. A couple of points:

    1) The figure#2 in the article shows that the dynamic REF current is much worse than the typical…

  • RE: About LT1461DHS8 Maximum Output Current

    Hi Naohisa,

    The 10mA is not necessarily the maximum current that the H Grade part can source. This is only the current range where the H Grade Load Regulation specified in the table will hold true for the whole temperature range (-40 to 125degC). This…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • ADI 全新中文资料(2019 年 2 月)

  • 【在线研讨会】电压基准源的产品及选择

    基准电压源是当代模拟集成电路极为重要的组成部分,它为串联型稳压电路、A/D和D/A转化器提供基准电压,也是大多数传感器的稳压供电电源或激励源,几乎在所有先进的电子产品中都可以找到。在近期的在线研讨会《电压基准源的产品及选择》中详细介绍了基准电压源的分类及工作原理和各类基准源的性能指标及主要的应用场合以及ADI的基准电压源的设计开发规划、产品优势以及对客户应用的价值所在。

    本期研讨会的回放请点击:http://www.elecfans.com/d/908063.html

    附件是本期研讨会的讲义,供大家下载并学习…