想知道,LT6604-2.5的增益是根据外部电阻来进行设置的。的最大增益可设置为多少?有没有增益与频率的曲线图?
with no impact or moving, adxl372 reads -15~15 [100mg] accelation range.
it’s about 1.5g, and i think it is big.
is this normal range?
and with just 1cm drop of pcb, the max peak reads 1300 [100mg].
i am confused if it is right value.
how can…
2009-10-03 15:49:15 linphone: G722 audiocodec
Andreas Neubacher (AUSTRIA)
Message: 80820
hi,
linphone is currently not supporting the wideband audiocodec G722, but i've found some several forum-entries about implementing this codec to linphone…
2010-06-15 15:30:38 request_irq(IRQ_UART0_TX) fails
Steven Vacca (UNITED STATES)
Message: 90327
Hi,
I have a BF-537.
In my driver, I am able to successfully request an IRQ for UART0_RX, request_irq(IRQ_UART0_RX), but get failure when trying to…
2008-03-01 15:15:07 Question about blackfin_cam.c
Frank Van Hooft (CANADA)
Message: 51957 I'm working my way through the blackfin_cam.c file as an educational exercise. I understand this is an example V4L1 driver, and the preferred method is V4L2…
2008-09-30 15:15:01 buildind uclinux from trunk
Omar Chanouha (UNITED STATES)
Message: 62949
My setup: toolchain, uclibc, dist = r1.5 on fedora 9. I make menuconfig and selected BF548-ezkit and then answered 'default' to all the config questions…
2008-01-15 15:42:35 network info at boot
ketan bhardwaj (INDIA)
Message: 49613 hello all,
Can we automate passing of network info such as IP, DNS, GW from uboot to kernel?
or how can we ensure that the previous settings remain after re booting also…
2009-07-15 15:03:33 SPORT I/O Speeds
Matthew Barousse (UNITED STATES)
Message: 77404
Hey All,
I have an ADC (AD7683) hooked up to SPORT0 and a DAC (AD5663) hooked up to SPORT1. As a simple system test I'm reading in samples from the ADC and formatting…
2009-06-15 15:25:47 BF537 ezkit lite & AD73322
Adrien Cottenceau (CANADA)
Message: 75750
I have a BF537 ezkite lite and a custom sound card on SPORT1 with 3 cascaded AD73322.
I'm using the Blackfin kernel driver AD73322, with some changes…
On an AD9915, bit 15:8 of CFR4 reads 0x21 after reset. But the Rev A DS states: "Requires register default value settings (0x31)" on page 36.
Which one is correct? Or should the bits read 0x21, but require 0x31 on writes?