The output signal…
Hi,
I've been modeling the LT6600-10 in the below circuit and the SPICE model outputs Vocm imbalance of +/- 20 mV. Is this correct and is there a way to mitigate it?
Thanks!
I'm currently using the LT6600-5 for a current sense resistor application, however and having some trouble with the design producing a wildly different gain than expected. The intended operation is for the LT6600 to amplify the measurements from a sense…
Hi,
we intend to use the LT6600-5 in a design where we need extended temperature range (-40°C to 105°C, preferably -40°C to 125°C). Device to be used as input amplifier for LTC2246H which is specified for -40°C to 125°C.
Datasheet…
I'm considering using a fully-differential amp like the LT6600 as a buffer amp for a DAC that has a differential current output. Normally, one would run the output from the DAC through a 200 Ohm resister to ground. For an op-amp like the LT6600, is…
Hi,
I am attempting to use some gain in the LT6600 chip to get lower noise output with a single-to-differential configuration that drives an ADC. The spec sheet says you can use 402 ohm Rs resistors (I'm using 470) but the circuit below oscillates at…
Hi bcom, it would be great if you can also add the exact value DB15-DB0 for those negative codes. Does the conversion look good for positive inputs?
Regards,
Lluis.
2008-10-10 10:30:52 L R Channel Swap in BF533
Appalayagari Sreedhar (INDIA)
Message: 63419
Hi,
Does anyone has implemented workaround for the anamoly L R Channel Swap in BF533.
05000265 -
- Sensitivity To Noise with Slow Input Edge Rates on External…
2010-05-10 10:07:10 在bf533-Ezkit上使用microwindows出错
进 王 (CHINA)
Message: 89283
大家好,我用的开发板是BF533-Ezkit,编译的内核文件是uClinux-dist-2008R1-RC8,配置好一切后现在板子上运行microwindows,出现如下问题,
root:/> nano-X &
175
root:/> m. Check kernel config
Cannot initialise…