Hi,
Can i left floating the shutdown pin? If i don't use a pull up resistor, will I have a problem about EMI?
Thank you.
Hi,
Can i left floating the shutdown pin? If i don't use a pull up resistor, will I have a problem about EMI?
Thank you.
In LT6200-5 OPAMP datasheet it is given that gain bandwidth product is equal to 800MHz at Av>=5. What is the maximum frequency at which LT6200-5 can be operated with proper rise and fall time.?
Is there is any method to improve the rise and fall time…
Hello,
I would like to ask you experts how to design the peripheral circuit parameters of the LT6200 for the loop filter of the ADF4401A?
Regards
Thank you very, very, very much for your reply. I am very happy to have your help.
Your answer confirms that what I need is HMC507. But I still have some questions to ask, please allow me to describe it in detail.
I need a 6.8GHz signal. The reference…
I downloaded this demo circuit from https://www.analog.com/en/design-center/evaluation-hardware-and-software/lt-spice-demo-circuits.html
When I attempt to run the simulation it never converges. Any suggestions? Thanks.
The demo is tilted "LT6200 & LTC2050…
Hi Anh,
My comment regarding 1% is just a conservative rule of thumb that I use. It's possible to achieve loop bandwidths that are greater than 1% of the 3dB GBW product. The AD8065 or LT6200 are a couple of op amps you might consider. Unfortunately…
Hard to say if it would definitely work, the purpose of the filter is to convert the charge pump current pulses to a steady tuning voltage, and it would take some testing to verify the architecture above as suitable. I cannot recommend that architecture…
Hi! I have some problems when using HMC4069 together with LT6200 and an external VCO(Crystek), i have an input signal of 40MHz. I set the N divider 2., and want to get signal of double frequency. I made the design using ADISimPLL, The bandwidth of LPF…
Hi,
See these links.
Ordering information can be found on the Sample and Buy section of the product pages.
Regards,
Jino
Hi,
See these links.
Ordering information can be found on the Sample and Buy section of the product pages.
Regards,
Jino