• About LT6106's Input


    Hello,

    I am considering LT6106 for current measurement.
    In the case of a one-way current path, I think that it is used with "+IN is connected to the load side".

    I am also thinking about the current flowing from the load side to VBATT.
    In the case…

  • LT6106 MTBF/MTTF data

    Hi

    Can you please give me the MTBF / MTTF for the part: LT6106HS5

    Best regards

    Joakim

  • About an input filter of LT6106

    Hello,

    Please let me know about the input filter of LT6106.
    The customer considers LT6106 by the following circuitry.
    However, the output of LT6106 oscillates it by this constitution.

    LT6106 behaves normally when I insert resistance between LT6106 and…

  • About LT6106 Vout(High) Output Swing High

    Hi,

    I would like to use LT6106.

    So, I have a question. Please help me.

    Question:

    I have a question about datasheet p.3.

    Below is the electrical characteristic about Vout (High).

    When Vsense = 120 mV, there is 1.2 V max (1.4 V at the whole temperature…

  • RE: Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN  and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application a

    Hi Manoj, 

    According the Absolute Maximum ratings of the LT6106, the inputs need to be kept within the supplies. 

    The AD8211 is pin compatible and looks like it could work in your configuration. Unlike the LT6106 though, its gain is fixed to 20V/V.…

  • Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN+ and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application as wh...

    Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN+ and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application as when…

  • RE: ADM4073F RS + / RS- Leakage problem

    Dear Kirill,

    Will the -IN / + IN of LT6106 have the problem of leakage voltage?
    If LT6106 is used to replace ADM4073F, can this phenomenon be improved?

    Thanks and best regards.

    Andy Yang.

  • RE: How to convert ADC reading to analog current value in LTC6106

    Hi shingeki1996,

    Apologies for the late response.

    For your test conditions, here is how I'd estimate what your 8-bit ADC output code should be given your schematic and that 3.3V is considered Full Scale with 172mA flowing through your sense resistor:…

  • RE: LT8410-1 Booster Circuit Current Draw

    Hello Dulcevida,

    Thanks for the quick answer. Please check my schematic below:

    The intention is the following:

    From a source that varies from 3.4 to 4.2V produce an HV_BIAS voltage that can be switchable between 53V and 105V. This is achieved by boosting…

  • RE: LTC6102 or Other Recommendation

    Hi ,

    In case you've not seen our parametric search for Current Sense devices, here it is.

    You can use the Excel filters to narrow down your search.

     XLSX

    Regards,

    Hooman