• LT Spice Model for LT6105

    Hi

    I like to know how can I get LT Spice model for LT6105. I could not down load it from the product support site. Shows up that model is available, but it is not active.

    Thx in advance

    Vince Hollo

  • LT6105 VOUT for the negative current

    In the datasheet page1, there is the typical application circuit and the equation for vout calculation.

    when the current flows in opposite(from load to source), vout is calculated in the negative voltage.s

    Judging for absolute maximum rating, vout hould…

  • LT6105 - Negative Voltage Rail Questions

    Hello,

    We are considering using the LT6105 current sense amp in our design to monitor a load that is being supplied by a -15v supply similar to the below diagram (this is from sheet 20 of the datasheet, the only change is that V+ is now 15V DC instead…

  • RE: Altitude related issues

    Dear Jon,

    thank you very much for your reply. Conformal coating will be used.

    Please, can you better explain the statement "Precision parts that might be subject to package strain"?

    Can this also affect the LT6105?

    Thanks in advance.

    Best R…

  • What's the minimum value of the Vsense in Current Sense Amplifiers?

    Hi, I want to sense a current which is  between a few hundreds of uA and 5mA.I'm not sure the minimum value of the Vsense in a Current Sense Amplifiers such as LT6105 or other suitable componets.  What's the value of the Rsense I should select? Is it…

  • RE: Circuit Oscillation Analysis

    Hi kaveh14934:   If you look at the INA193 data sheet, its CMRR range over temperature is "12V to 80V".   So it does not include ground.  In your circuit, when the command is to go to zero current, the input CM to the INA193 drops to ground.   I think…

  • RE: LTC4125 - DC2770A-B-KIT - PTH1

    Hi Andrea,

    Setting IMON at 1V is a good way of setting the transmitter with fixed duty cycle. Instead of setting PTH1 voltage directly, I recommend you use PTHM pin to set up the duty cycle. Some protection features are only in T3 (please refer to Figure…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…