• LT6100 Vout unusually high voltage when no current?

    Hey all,

    I've got a design utilizing a LT6100 to measure current being provided to a connected load.  The LT6100 is configured for a total gain of 25.  Under normal circumstances (when there is actively current moving across the sense resistor) there…

  • Regarding the use of LT6100 for Current Sensing & Application Note 105 December 2005 Page Number 60,61 [ Requirement is for Low Current Sensing]

    Hello Friends,

    In the LT6100 The range for Vs+ and Vs- is from 4.4 to 48V. We are putting it towards the ground. Instead of monitoring high sensing current I want to monitor the low sensing current.

    If I have voltage close to 0V or 500mV will it be able…

  • LT6100 reliability MTTF

    Hi there,

    I'd like to use the LT6100 in an application requireing functional safety. Where can I find the Mean Time to Failure (MTTF) of the part?

    - Karsten

  • LT6100 supply voltage

    Hi Experts,

    I am using an LT6100 for high side current sensing. My current measurement range is very wide, from 20mA to around 700mA. I am using a current sense resistor of 0.75 ohm for sensing and the sense inputs are driven by +34V supply. I have set…

  • LT6100

    Hi

    I have a question LT6100.

    In the recommended circuit of the LT6100, when using at 24 Vin,
    How much can it be thought that the withstand voltage of the 220 pF ceramic capacitor of Pin 3 is required?

     

     

    Best Regards

    HOD

  • RE: LTC6102 or Other Recommendation

    Hi ,

    In case you've not seen our parametric search for Current Sense devices, here it is.

    You can use the Excel filters to narrow down your search.

     XLSX

    Regards,

    Hooman

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…