• LT5537 Input Matching Network

    Hi all,

    Following is the datasheet 9 page ~ @ LT5537,

    Input Matching

    The 1:4 input transformer can also be replaced with a narrow band discrete balun circuit using three components as shown in Figure 6.

    Capacitors C11, C12 and inductor L1 form a tank…

  • The VOUT vs PIN transfer raw data or curves of LT5537

    Hi Sir,


    Our design needs LT5537 the VOUT vs PIN transfer curves which like the following or raw data.

    Frequency are 100MHz, 200MHz, 400MHz, 600MHz, 800MHz and 1GHz.

    Input power range is -100dBm to 20dBm.


    Could you help us provide the information?

  • LT5537 output voltage curve raw data when frequency in 1GHz

    Dear Sir,

    Customer wants to know the output voltage of below table, When Frequency in 1GHz. Could you please help provide the raw data of below curves? Thank you.

    DCV on
    RF_Lvl (V)
     
    dBmV
      30
      25
      20
      15
      10
      0
      -10

    Yen…

  • Peak power vs log and envelope detector

    Hello, i need to accurately measure a AM SSB signal peak power at a frequency starting from 1.5 to 30MHz: according to you it is better to use the ADL5910  or a log detector like LT5537 or the LTC5507? For me it is important the temperature behaviour,…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…