• RE: LT4256-2 output short test problem

    Dear Ritesh,

    Thanks for your support.

    I have other questions about LT4256. I am using LT4256-1, not LT4256-2.
    R1068 I used 3 resistance values for testing. The test conditions are a bit different from previous tests. The previous test output short-circuit…

  • LT4256 gets over heated

    Have a small doubt regarding LT4256 Hot swap controller.

    Our schematics is similar to what is being shown below. However, we have one more Power domain(Vsys) powering Vout.

    So even when Vin is OFF, the Vout will still have a voltage as per the Vsys…

  • LT4256 hot swap controller enable/disable

    Has anybody used the LT4256 hot swap controller as an electronic circuit breaker? I have simulated and designed a board that is essentially identical to the evaluation module (resistor scales are different due to different source voltage). I am trying…

  • Hotswap with remote sense: any solution superior to the LT4256?

    Dear Power by Linear,

         I have an application where I need to use a hotswap device to prevent my source (a power module) from going into current limit when a large MLC capacitor bank is switched in. The hotswap is for constant current charging of the capacitor…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh