• LT3958 inverting converter layout

    I am using LT3958 in the Inverting configuration. I would like to know if there is some diagram of the recommended layout for this configuration.

  • LT3958 Inverting converter soft start

    I am doing some simulation vs data sheet checks with this part in an inverting configuration. With a 68nF capacitor on SS pin, Tss (page 13 of data sheet) gives 8.5ms soft start time but simulation gives ~5ms. In fact, if I consider only the rising part…

  • LT3958配置为反相转换器时电感的连接方式

            上图是LT3958配置为反相转换器应用电路,那两个电感推荐型号是DRQ125-220,查过这个电感数据手册之后发现它是四个引脚双电感,可以连接配置为下图三种模式,双耦合电感、串联和并联三种,根据原理图我应该连接为哪种模式?上图中L1A和L1B是两个独立的电感吗?还是一个电感连接为双耦合电感模式(下图中Dual Inductor)?

  • Use the SS input to limit input current

    I want to use the LT3958 boost converter

    24V input and 70V output.

    Most important, the input current shall never exceed 1A at 24V, even when this means reducing the voltage at the output.

    Can I use the SS (SoftStart) input to do that?

    I have used…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032