• About LTSpice Simulation of LT3932

    Hello Analog,

    I am using LTSpice to optimise component parameters for the LT3932 Buck LED driver in preparation for a new design.

    The model mainly works well, however I have found that the EN/UVLO pin does not respond to falling voltage.

    From the datasheet…

  • RE: LT3922 Buck Mode LED Driver

    Thank you for the reply and the advice to use the LT3932. Somehow It was not suggested although I was looking exactly for this kind of controller, I guess the LT3922 is just more popular. Maybe a hint, next to the example application in each controller…

  • RE: Rise time speed for LT3762

    After poring over Linear Tech datasheets, it seems that the part we want is the LT3932. It is specifically designed for LED flash applications and apparently can support a very long (essentially infinite) PWM off-time and will supply full current to the…

  • RE: LT3518 Short-Circuit

    Hello Martin,

    The LT3518 is not designed for short-circuit protection.

    More recent ICs such as the LT3922, LT3795, LT3762, LT3932, LT8391A and other LED drivers now have the short-circuit protection which you are looking for.

    I hope this helps,

    KSz

  • RE: ADI官网史上最大合并升级完成,有奖邀你来体验

    最近关注单片、同步、降压型 DC/DC 转换器LT3932,该器件具内部 36V、2A 电源开关和一个内部 PWM 发生器。其固定频率、峰值电流模式控制能针对高达 2A 的 LED 串准确地调节电流在 ±1.5% 内。其集成的 PWM 发生器提供 128:1 调光比。如果需要高达 5000:1 的调光比,那么 LT3932 和一个外部 PWM 发生器就可适合这类应用。LT3932 的 3.6V 至 36V 输入电压范围非常适合多种应用,包括汽车、工业和建筑照明。其 Silent Switcher

  • RE: LT3932 (DC2296A) long time PWM off and start up delay

    Hi Osamu,

    When using the LT3932 for flash applications, the first "flash" pulse is used to help the part find where to regulate the following pulses, but isn't a perfect pulse itself (hence the long rise time). In a well designed system, the following…

  • RE: LEDs that drive higher voltages on the LT3932 do not flash properly

    Customer went for offline support. Considered close.

  • RE: About LT3475 Parallel Connected 3A Output Circuit

    Hi Naohisa,

    Dimming at microsecond intervals is extremely fast for PWM dimming. If you consider a pulse with a 2 microsecond period, that's 500kHz dimming. Even operating the LT3475 at 2MHz switching frequency there wont be many switching cycles to regulate…

  • 关于LT3932驱动较高电压的LED不能正常闪烁

    我使用DC2286A这个LT3932的评估板给一个12V,2A的LED供电并且处于PWM触发模式,但是经过1S后,我提供一个脉冲到评估板,LED却不能正常闪烁。我已经把板子上的R7更换为130K以便输出高电压。和网站的模拟对话中描述的不一致。www.analog.com/.../led-driver-for-high-power-machine-vision-flash.html

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032