• ADA4627-1 and ADA4637-1 Null Inputs Connection

    Hi,

    ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?

    Regards,

    Ivan.

  • 2 CVBS+1 LVDS input ->1 LVDS output ?

    Dears,

    Does ADI have the solution that support 2 CVBS and 1 LVDS(5 wires) input then 1 LVDS output?

    The CVBS signal is from camera and the  LVDS is from video or navigation.

    The output LVDS will display in 800x480/1024x600 screen.

    This is the siganal…

  • Powerful Combinations are Possible when 1+1>2

    It’s a new beginning for Analog Devices and Linear Technology. Together we become the high-performance analog industry leader with an innovation engine fueled by our comprehensive portfolio of analog and mixed signal products and solutions.

    We have…

  • ADA4310-1, 4311-1 with sloped PD0, PD1

    When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive…

  • 1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this?

    1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this? asked by Robert B.

  • AD8195:  1:1 HDMI/DVI Buffer with Equalization

    Is there any documentation for the evaluation board for the AD8195?

    Thanks,
    John

  • Differential video transmission with ADA4433-1 and ADA4830-1

    Hello,


    Thanks for providing the spice model of both ADA4433-1 and the ADA4830(-1).

    I'm trying to design a DC coupled differential transmission system using the ADA4433-1 and the ADA4830.

    The overall gain from input (ADA4433-1) to output (ADA4830…

  • LTC5588-1 and LTC5586 IBIS model

    Hi Experts:

    Could you share LTC5588-1 and LTC5586 IBIS model for simulation, thanks!

  • LTM8055 and LTM8055-1

    Dear Team,

    We are using LTM8055IY#PBF in our production.

    Since lead time of this item is high, for the same design we plan to purchase LTM8055IY-1#PBF as a drop in replacement whose stock is available.

    The only difference that I understand between LTM8055IY#PBF…

  • How to configure 1 TX-1 RX in No-OS

    Hi all,

        My design uses ADFMCOMMS2 module and ZEDBOARD, I want to transmit data using 1 TX- 1 RX but the default set 2  TX-2RX in No-OS, so what parameters in  default_init_param in main.c file I need to modify in order to  set 1 TX- 1 RX, thank you for…