Hi,
I would like to know about the absolute maximum ratings of FB pin on LT3799-1.
According to the datasheet, the positive max is 3V. How about negative? Is that -3V?
Thank you in advance.
Regards,
Koide
Hi,
I would like to know about the absolute maximum ratings of FB pin on LT3799-1.
According to the datasheet, the positive max is 3V. How about negative? Is that -3V?
Thank you in advance.
Regards,
Koide
Hello!
can the LT3799 be used as a dc converter with ac input?
Apparently, a TM PFC regulator in voltage mode can convert ac to dc through a flyback operation- pretty similar to LED circuit but the pure dc regulator must regulate the output voltage.
…Hello,
I tried to simulate the LT3799 being driven by 50 Hz supply, not the 600 Hz as in the Linear's example (jigs).
The input current did not follow the input voltage at 50 Hz, just the opposite as it was at 600Hz.
Why is that ?
Is the PFC is depended…
Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:
[Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
.file_attr 1="1";
syntax error is at or near text '1'.…
Greetings!
I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…
|
Hello,
In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?
Best Regards,
Hello Team.
1:1 transformer applied in IF pin is expensive.
so we want to use without transformer.
is it possible that?
Can you support solutions?
thanks.
Best regards,
Josh
I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…