• LTC6908 Compatibility with Various Converters

    I am investigating using an LTC6908 in an application with multiple power converters. In this application, it would run at a nominal frequency of 560 kHz (504 kHz to 616 kHz with spreading). I am hoping to confirm that all the converters that will be…

  • LED Driver Implemented as Constant Current Battery Charger

    I am designing a battery charger for an existing battery pack design of 28 11000mAh NiMH cells.  The goal is to design a charger with a constant current output of 3.0A with low DC ripple.  The LT3795 and LT3796 Drivers seem to be a good fit for my application…

  • RE: Constant Current Source Design which can source 20A current

    Hi FormerMember

    In LTC3779 data-sheet it is mentioned, " Constant-Current Regulation (IAVGSNSP and IAVGSNSN Pins)The  LTC3779  provides  a  constant-current  regulation loop for either input or output current. A sensing resistor close  to  the  input  or 

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032