• RE: LT3791-1 - EMI

    Hi Vagelis,

    EMI can be complicated with causes from component choices to board layout. It is very design dependent. I recommend that you contact ADI FAE in your area to help you out. 

  • lt3791-1 I want to know the difference between input voltage and output voltage when boosting.

    Hi
    A step-down and step-up circuit was constructed using the LT3791-1.
    The output current up to 2A worked well without any problems.
    However, when the input voltage and current are supplied at 12V / 10A,
    If the output voltage and current are more than 24V…

  • RE: 100 W LED Driver [ LT3791 ] - Design assistance needed

    Hello,

    I am looking at the layout and I see a problem. where is the solid, high power connection between the MOSFETs and the sense resistor?

    Would you like customer support without the public forum to keep your design private? If so, please send email…

  • RE: .file_attr 1="1";

    Hi Gideon,

    Sorry for the delay in responding.

    The cause of the problem is "-file-attr CORE0" and "-DCORE0" both being included on the compiler command-line. Could you delete CORE0 from the "Additional attributes" in Tools Settings > CrossCore Blackfin…

  • 18 cells BMS with (LTC6813-1) and active balancer LTC3300-1 x3

    Dear Friends,

    We are planning to make 18 cells BMS with bidirectional active balancer. In order to that we are considering LTC6813-1 as 18 cell battery stack monitoring and LTC3300-1 x3 for link with active balancer. I have a few questions to clarify.

  • ltc6811-1 with ltc1380 multiplexer

    I'm trying implement LTC1380 with LTC6811-1 for temperature sensors. GPIO1 is used to take analog reading. how should I write data to comm register? And how to read analog read from GPIO1?

  • LTC6810-1 Number of cells

    Hello,

    I want to monitor 4 cells using LTC6810 is it possible? The manual never shows any example to connect less than 6 cells.

    -Mark

  • LTC6810-1 communication problem

    Hello everyone,

    I have trouble in SPI communication with LTC6810-1. The chip is standalone and is connected to STM32 microcontroller via SPI interface. For now, I need to determine the communication itself.

    I have sent simple communication frame "00 01…

  • RE: LTC2955-1 auto-turn-on disabled with 1 second VIN removal

    When you remove the Vin (battery) for LTC2955 and plug it back in, you do not get tEN(LOCKOUT). That's like power cycling the part and you have to go through the complete turn on sequence.

    Instead try using KILL signal or ON signal to turn off the…

  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…