• LTC7060 for >60V synchronous application

    since LTC7060 has floating ground and inverting input logic feature. is there any application using LTC7060 for LED driver like LT3756 or LTC3783.

    I feel it can upgrade these non-synchronous boost regulator to synchronous one. can it work for these app…

  • RE: Looking for LED driver for 100W 70-75V 2A LED from 9-12V sourc

    Hello Burhan,

    The LT3756-2 is the correct IC for you.

    You need to run at low switching frequency to limit high voltage switching losses. I recommend as low as possible.

    The current will get rather high, so a large catch diode for high current and high…

  • RE: Constant Current Source Design which can source 20A current

    Hi FormerMember

    In LTC3779 data-sheet it is mentioned, " Constant-Current Regulation (IAVGSNSP and IAVGSNSN Pins)The  LTC3779  provides  a  constant-current  regulation loop for either input or output current. A sensing resistor close  to  the  input  or 

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032