Hi ADI Pals,
Does LT3748 meet our in/out requirement as
Voltage input 19VDC, voltage output 55VDC, output current ~600mA (30W) to meet the 802.3AT PSE application?
Thanks.
Hi ADI Pals,
Does LT3748 meet our in/out requirement as
Voltage input 19VDC, voltage output 55VDC, output current ~600mA (30W) to meet the 802.3AT PSE application?
Thanks.
Hi everyone,
The IC shortage seems to be getting to my design again.
I need a replacement for the LT3748. I used two of these devices to generate isolated rails.
My input supply was 12V.
The output of converter 1 was 12V, 1A
The output of converter…
Evening everyone,
I'm seeing some issues with the LT3748. Here is the schematic of mine:
This is the transformer: https://www.mouser.co.za/ProductDetail/Wurth-Elektronik/750310617?qs=%252BUQ4csG8Rscr4kcgwycPjw==
At the output of this I have the…
Good Day,
Please carify when do you suppose to prepare the simulation jig for the LT3748?
Hi, I am having some problems getting a design based on the LT3748 to regulate. The input is 12V and output should be 5V,
Examining the scope output at the FET drain point it seems that the boundary mode condition is not being detected. The voltage at…
Hello Team,
We have designed flyback converter with LT3748. We want output to be 48V with 1.4A capability.
Please find attached schematic of LT3748 Flyback converter. We have done the simulation and simulation circuit works fine.We have used Wurth transformer…
Hello
I am using LT3748 for PoE supply generation.
Below is my circuit:
I am testing this circuit.
I am not getting any output.
Is any wrong connection to INTVCC pin?
Hey everyone,
Can someone please provide me with an app note or info on how the following is calculated:
Hi,
I would like to design LT3748 Isolated power solution to our PoE PSE source.
Following is our specification:
Vin: 14V (+-) 10%
Vout: 48V@250mA
There is a reference design on ADI website(see following link), but its transformer size is too big to fit…