• LT3484-1 Direct Alternative

    Hello,

    I notice now that the LT3484-1 is not freely available.

    Can you please urgently advise if there is an alternative available (Ideally with the same footprint)?

    I found the LT3468 to be available, that seems to be a good alternative but footprint…

  • RE: Question about LT3484

    Hello Fil,

    I have an application with the LT3848-1 and am contemplating using the same transformer as Keita and Piro_gue.

    The specs of the  ATB322524-0110-T000 seem to match the 3484-1 well, except for the primary inductance. (3484-1 recommends >10uH…

  • LT3484-1 current limitation

    I'm designing a capacitor charge circuit using the LT3484-1.  Its average current draw during charging is stated to be 225 mA however the instantaneous current can be as high as 550 mA.  If I'm looking to power this from a USB port say, where the current…

  • RE: LT3483负向转换器的问题

    LT3484这个型号目前在咱们的全球技术社区可以获得技术支持哈,到这儿提问吧~https://ez.analog.com/power/

  • RE: 450V with 1mA generation from an input voltage of 5V to 12V input

    Hello Bilvin,

    have you checked out the LT3751 yet?

    Linear Technology - Product Page 

    Its intended to charge capacitors to large voltages and offers plenty of power as controller. When 450mW is all you're asking for the integrated parts like LT3484 could…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032