What is the input resistance of the LT3482 CTRL pin? From an LTSpice simulation, I would expect around 1 GOhm. Is this a realistic value?
What is the input resistance of the LT3482 CTRL pin? From an LTSpice simulation, I would expect around 1 GOhm. Is this a realistic value?
Hi,
I need a voltage inverter for LT3482, which will take the variable Vout from it and convert to -Vout for biasing a photodiode device. Would you recommend a product or would it be a better solution to use LT8362 with variable resistor and current…
Hi,
I'm trying to use a LT3482 to generate 58.6V.
I'm using a voltage divider with 465k and 10k which should give ~ 58.6V but actually gives ~ 52V.
Measuring the resistance of the 465k when on the board gives 425k so it looks like this is…
We're looking at the LT3482 as a solution for powering an APD and monitoring the current. All of the design examples (and the eval board) show the feedback connected before the power goes through the current mirror - but the drop through the current mirror…
I don't this this is capable to do high voltage output as you require. You may check the part numbers mentioned in separate that you asked. https://ez.analog.com/power/f/q-a/166675/voltage-inverter-for-lt3482
Dear Lolomontp,
The parts you have chosen all can have the output noise filtered, but they have different capabilities.
You can eliminate the lt3482. You do not need the high voltage capability, since your output is quite low.
i have a few questions…
Hello Mr. Intelesano,
You are correct in that LT3482 will not deliver the current you need.
If your converter "must" operate from a minimum input source of 3V, it will be difficult to achieve a simple boost approach. For a 20mA load I would…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |